Part Number: TCA9535
Other Parts Discussed in Thread: TCA6424, TCA6416
We are using AM64xx with TCA9535 IO expander which is connected to main i2c0 bus.
Please share the device tree configuration with correct driver compatible string for TCA9535.
&main_i2c0 {
pinctrl-names = "default";
pinctrl-0 = <&main_i2c0_pins_default>;
status = "okay";
exp1: gpio@20 {
compatible = "ti,tca6424";
reg = <0x20>;
gpio-controller;
#gpio-cells = <2>;
gpio-line-names = "GPIO_eMMC_RSTn", "CAN_MUX_SEL",
"GPIO_CPSW1_RST", "GPIO_RGMII1_RST",
"GPIO_RGMII2_RST", "GPIO_PCIe_RST_OUT",
"MMC1_SD_EN", "FSI_FET_SEL",
"MCAN0_STB_3V3", "MCAN1_STB_3V3",
"CPSW_FET_SEL", "CPSW_FET2_SEL",
"PRG1_RGMII2_FET_SEL", "TEST_GPIO2",
"GPIO_OLED_RESETn", "VPP_LDO_EN",
"TEST_LED1", "TP92", "TP90", "TP88",
"TP87", "TP86", "TP89", "TP91";
};
}