Part Number: SN75DP126
Hellow.
Does it support input/output interface as below?
- INPUT: HDMI
- OUTPUT: HDMI 2port

Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN75DP126
Hellow.
Does it support input/output interface as below?
- INPUT: HDMI
- OUTPUT: HDMI 2port

Thank you.
Hello,
For DP++ to HDMI, you can use DP158 (Re-driver) or DP159 (Re-timer).
Thanks,
Zach
Hello,
Thank you for the reply.
If the input/output is as follows, is there any problem if it is designed as shown in the block diagram?
- Input: DP++
- Output: HDMI 2port(cloned)

DP126 and DP159 are used.
Thanks,
Hello,
Dp126 is a mux, it can only support one HDMI port at a time.
You will need an HDMI splitter if you would like both HDMI output simultaneously.
Thanks,
Zach
Hello,
I would like both HDMI output simultaneously.Thanks for pointing it out.
Please recommend a 2-channel output HDMI splitter TI product.
Thanks,
Hello,
You are welcome.
Unfortunately, we do not have a HDMI splitter solution.
Thanks,
Zach