Other Parts Discussed in Thread: SN75ALS1178, , SN65C1168E, SN75C1168, SN65C1168
Dear Specialists,
My customer is evaluating SN75ALS1177NS as a replacement for SN75ALS1178.
They have a question about current consumption.
I would be grateful if you could advise.
---
We are evaluating to use SN75ALS1177NS as a replacement for SN75ALS1178NS .
The current consumption of SN75ALS1177NS is small.
ALS1177NS About 15mA at standby, about 35mA at 2.5Mbps operation
ALS1178NS About 40mA at standby, about 60mA at 2.5Mbps operation
The datasheet shows no difference in current consumption between the SN75ALS1177/1178.
question)
When comparing the current consumption Icc and other AC characteristics of the SN75ALS1177 and SN75ALS1178, which one tends to be larger or faster?
Could you please let us know some possible causes?
---
I appreciate your great help in advance.
Best regards,
Shinichi