Part Number: DS90UB947-Q1
Other Parts Discussed in Thread: USB2ANY
Hi,
my IVI has two display port, the one use 941, the other use 947. the display panel use 948, the two display port use the same deserializer 948,and the same resolution,1920*1080.
now,941-948,link ok, display ok.
with the same panel, 947-948, no display, link is not stable, 947 indicate "back channel CRC error",how can I solve the matter?
when I connect usb2any to 947's I2C, the I2C communication may be No ACK, the link of 947-948 is very diffcult.why?

thanks for help!
the best regards!