Part Number: TCAN1145-Q1
Other Parts Discussed in Thread: TCAN1146-Q1
Hello expert,
I'd like to know about the detailed behavior of TCAN1145-Q1 with selective wake up.
Based on Figure 10-11's Sleep mode (selective wake enabled), WUP and WUF is required to transition from sleep mode to standby.
However, based on not at Figure 10-11, it said "NOTE: Upon a wake event, WUP (SW off), WUF (SW on), LWU, the device will transition into Standby mode"
The NOTE seems it can move from sleep to standby based on WUP "or" WUF.
Then, Is WUF mandatory moving to standby mode or will TCAN1145-Q1 move to standby when it receive WUP and Selective wake is enabled?
Also, Figure 10-11 don't have description regarding INH.
Based on other description INH will become High when WUP received.
Then, will INH become High when WUP received during selective wake is enabled?
Best regards,
Kazuki Kuramochi