Part Number: SN65DPHY440SS
Hi All,
We have a FPC design which is of 6.5inch length for the camera since we are crossing the CSI-2 FPC cable length max constrain we used SN65DPHY440SS to retime the CSI-2 signal.
Attached the schematics for your review and reference.

Camera is not functional with this re-timer.
We have tried all the possible configuration using the pull-up/down resistors that this chipset supports in hardware.

We need support on bringing this FPC cables working with the re-timer.