Part Number: TCA9535
Other Parts Discussed in Thread: TCA6507
HI.
Currently in a project application due to the limited number of GPIOs in the MCU, I would like to use the TCA9535 to expand the GPIO ports. This GPIO is used to drive a high side switch (e.g. IN port of TPS48111-Q1,) which is using a PWM output but at a frequency of about 100 HZ. By reading the link (e2e.ti.com/.../ 1211795/tca9535-could-tca9535-be-used-to-simulate-pwm-output?tisearch=e2e-sitesearch&keymatch=TCA9535#) should be possible. My question is that if I use the TCA9535 to output PWM at 100Hz, then I have to use the IIC to control the GPIO flip-flop all the time during the 10mS cycle, instead of using the MCU's GPIOs directly to set the PWM frequency and then the GPIOs will keep outputting the corresponding PWM waveforms. Is my understanding correct? Thank you.