Part Number: TUSB501
Hi, Ti expert.
The customer is reviewing the use of TUSB501 for the Kiosk under development.
Customers have inquiries regarding placement when applying TUSB501 (Redriver).
The structure of the terminal/device is as follows:
The customer wants to use the USB3.0 line of the 4CH USB HUB of the MAIN PCB between the USB3.0 and GIGABIT Ethernet connections via 'BTOB CON ← FPCB → BTOB CON of the SUB PCB'.
Q1) Accurate use of EQ, DE, OS and how to select setting values?
Q2) The customer asks which side of the TX+- / RX+- line the TUSB501 (Redriver) should be placed close to when performing PCB Artwork.
(Installation location of USB3.0 Redriver (which side should be installed closer to the host or B to B connector?)
Q3) Please check if there is any guide document?
Please check. Thank you.