Part Number: DP83867CS
Hello experts,
I would like to perform an SI analysis of "DP83867CSRGZR" in SGMII.
I have downloaded the IBIS model from the product page of "DP83867CSRGZR".
However, the IBIS model does not have a differential line for SGMII, so ADS defines it as a single-ended line as shown in the figure below.
Is there any problem with SI analysis of the SGMII differential line?

Figure1 FPGA_TX_DP83867_RX
In addition, the SGMII differential output pins in the IBIS model do not have the word "SGMII" on them.
Is the pin configuration correct as shown in the figure below?

Figure2 DP83867_TX_FPGA_RX
Thanks and best regards,
Shinigo Ozaki