Part Number: DP83TG720R-Q1
1) The SNLU289 eval board has no pin strap resistors on RX_D0, RX_D1 & RX_D2. So these lines would all be open at boot (MAC[0], MAC[1] & MAC[2] would all be 0). According to table 8-18 of the DP83TG720R-Q1 datasheet this is a reserved state ? Can you confirm it is acceptable to have no pin-strap resistors on these lines?
2) If these boot strap resistors are required, do you have any placement guidance - I am concerned these resistors would create a stub on a high frequency transmission line - which doesn't sound like a good idea.
3) Is there any best practice guidance on whether TX & RX RGMII alignment is done at the PHY, the MAC or at the PCB traces?