This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS320PR810: I2C secondary mode

Part Number: DS320PR810


Hi,

In figure 8-4, mode pin needs 59kohm for 16lane/i2c secondary mode.

However, in pin description, mode pin needs 24.9kohm for i2C secondary mode.

Could you explain why these are different?

After connect external I2C to redriver SCL/SDA, SCL/SDA of redriver is pull-down.

Could you provide any guide for this issue?

Thanks.

  • Hi David,

    Please refer to the pin description for MODE to configure the device with the correct strap settings. Figure 8-4 references an incorrect strap value.

    For I2C secondary mode on the DS320PR810, the correct resistor strap setting would be 24.9k to GND.

    Best,
    David