Part Number: TIOL1123
Hello,
regarding to the datasheet page 19, TIOL1123 is capable of withstanding up to 1.2 kV of 1.2/50 – 8/20 μs IEC 61000-4-5
surge with a source impedance of 500 Ω.
IEC61000-4-5 states to use 2, 12 or 42 Ω as source impedance.
Is there any specific reason why the 500 Ω are used?
Thanks & regards,
Jonathan