Part Number: TCA9548A
Other Parts Discussed in Thread: TCA9803
Hi all,
I would like to ask a question of configuration.
Is it possible the output configuration as shown below?
Vcc is 3V.

Best Regard,
Ryusuke
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Ryusuke-san,
Yes, this is the intended operation of this device. You can also see some additional explanation in section 9.2.1 Design Requirements in the device data sheet which describe the supply requirement that you've met.
Best,
Danny
Hi all,
Thank you for your reply.
I would like to drive up to about 5meters cable length.
In such cases, should I use TCA9548A with an I2C buffer like the TCA9803?
or only TCA9548A?
I think using a buffer to improve connection stability.
Best Regard,
Ryusuke
A 5 m cable definitely needs strong buffers. Please note that the B side of the TCA980x must not be connected to such a switch. And depending on the cable's characteristics, the total capacitance might exceed the I²C limit of 400 pF.