Part Number: SN65HVD01
Hi Support,
We use SN65HVD01 IC on my project, we will generator the signal and connect to pin 5 of SN65HVD01.
According to IC spec, the VIL range is 0~0.3*VL (VL is 3.6V) ==> 0~1.08V, we have measure the waveform as follows:

If we use "min" of oscilloscope, the value is -0.18V, it will be over the spec requirement,
so we want to confirm it, the SN65HVD01 spec requirement is "min" or "low" of oscilloscope?
thanks.