This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Support,
We use SN65HVD01 IC on my project, we will generator the signal and connect to pin 5 of SN65HVD01.
According to IC spec, the VIL range is 0~0.3*VL (VL is 3.6V) ==> 0~1.08V, we have measure the waveform as follows:
If we use "min" of oscilloscope, the value is -0.18V, it will be over the spec requirement,
so we want to confirm it, the SN65HVD01 spec requirement is "min" or "low" of oscilloscope?
thanks.
Hi Ming-Tung,
Clemens is correct - a little bit of overshoot/undershoot is harmless and it could be a measurement artifact.
With that being said:
1. The absolute minimum on a logic input pin (like pin 5) is -0.3V, so -0.18V is greater than absolute minimum so the part will not be damaged.
2. The VIL spec is a rec. condition so it will be a bit more strict than absolute max/min conditions - however the low undershoot will not cause a false bit - the device will still read that as a low.
Please let me know if you have any other questions!
Best,
Parker Dodson