Other Parts Discussed in Thread: SN65HVD01
Questions about the SN65HVD01 part:
1. Can it be used as a standard RS-422 transceiver?
2. Do you have a full-duplex version of it?
3. If ans of #2 is no, do you recommend someone to use two SN65HVD01 parts to form a full-duplex channel?
4. Can this part be run at 500kbps?
(The 1.8V I/O logic is needed to interface with the Xilinx V7 part. However, please also recommend other good full-duplex RS-422 transceivers, and the I/O can be level translating from1.8V I/O to other voltages. Thanks)