Tool/software:
What happens if I communicate using two SN65HVD01s and set different speeds for each?
If I set IC 1 to 250kbps with SLR set to VL and set IC 2 to 20Mbps with GND, will communication work?
Or, if set to GND, it is set to 20Mbps, but can communicate at 250kbps. Will there be a problem if both SN65HVD01 are set to GND and communicate at 250kbps?
Is it possible to change the firmware to change 20Mbps to 250kbps for communication?