Other Parts Discussed in Thread: THVD1500, THVD1410
Hi Sir
May SN65HVD01 can take signal from RJ45 and the get Differential signal transfer to Single-Ended?
or there have other suggestion part?
Bogey
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Apparently, these signals are designed to work with any RS-485 receiver.
The SN64HVD01 does not work at 5 V. Do you actually require a 5 V output (as implied by the image)?
What frequency do you need?
The cheapest single-channel receivers are the THVD1500 (5 V) or THVD1410 (3.3 V).