Part Number: TUSB2036
Other Parts Discussed in Thread: TPS65988, TUSB8044A, TUSB4041I, TPS55288
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB2036
Other Parts Discussed in Thread: TPS65988, TUSB8044A, TUSB4041I, TPS55288
Hi,
Do you have a block diagram that you can share?
With USB Type-C, the Power Role and Data Role are now two separate functions. For example, you can be a Data Source which being a Power Sink, or Data Source and Power Source. The roles can also be swapped as needed. Both the data role and power role are handled by the PD controller.
With TUSB2036 hub, the hub downstream ports will always acts as a USB source, it can not act as a USB sink. Are you trying to connect the tablet to the upstream or the downstream of the hub?
Thanks
David
Hello. From what I understand about the protocol, I agree that a USB host can be a power sink. I am just having a hard time interpreting USB hub specifications to understand if they support that and are relevant to my system's use case.
With TUSB2036 hub, the hub downstream ports will always acts as a USB source, it can not act as a USB sink. Are you trying to connect the tablet to the upstream or the downstream of the hub?
Okay, good to know. If I'm understanding hub functionality correctly, the tablet should be upstream of the hub. Here is a block diagram showing the main use cases I need to handle (Charger plugged in, charger unplugged). CONFIG A

As you can see in the simplified block diagram above, the controller would require two USB devices to connect to it.
This other configuration (CONFIG B) would also be acceptable:

In config A the controller would take in two usb devices. In config B it would only need to handle the tablet. In either case, the tablet needs to go into power sink mode (always trying to charge), data host mode. I wanted to see what controller options we have to make this work. The ideal would probably be config B since it would be a smaller hub. The key for us would be if the controller can automatically place the tablet into power sink, data host mode (i.e. minimal programming).
I apologize for any strange things/inconsistencies in the block diagram, as it is quite simplified. The power input for our system also has a battery backup, so disregard the config b, charger unplugged 0V input. Please let me know if anything needs clarification
Hi,
I am sending this question to our PD controller team for their input, I think for this particular case, you would need a PD controller such as TPS6598x controller.
Thanks
David
We sort of prefer to lean on a simpler option if possible. Ideally one simple one that manages the tablet. But im interested in hearing what options are available for either configuration.
Sorry about delay, this thread got misplaced in the system.
Yes, TPS65988 would be right solution here. TPS65988 is a dual port device. You need a dual port PD controller to negotiate PD on two different ports.
What options for configuration B where we would like a simple programmable or preprogrammed/state machine USB Hub to negotiate simply to host mode + charge mode? Im looking for something resistor settable or that automatically negotiates the tablet to data host + accepts charge.
For configuration A that seems like the right solution, thanks. I want options for configuration B too..which would be a good amount simpler for us.
Hi,
Can you please take a look at TUSB8044A, https://www.ti.com/lit/ds/symlink/tusb8044a.pdf and in particular section 8.3.1 Battery Charging Features to see if the hub meets your design need?
Thanks
David
Before I go too crazy looking into this chip..is there a USB2 only "version" of this chip. The TUSB8044A is quite a behemoth for just using it in config B in the block diagram i sent.
To clarify I'd like something that automatically places the tablet into a DFP (downstream facing port) and SINK. With no programming or at least resistor settable to configure it.
Reading through the TUSB4041I it doesnt seem to allow USB charging support for the upstream port.
Hi,
We do not have a hub that can support USB charging for the upstream ports.
Thanks
David
In that case, is a configuration like this possible?

Is there an IC that can autonomously place the tablet into SINK mode while the tablet continues as data host role?
Hi,
When you say SINK mode, I assume you want to be in POWER.SINK mode?
Thanks
David
Hi,
I think you would need a PD inside the tablet as well. The PD will configure the tablet as DATA.SOURCE and POWER.SNK. The IC will be another PD that will configure itself as POWER.SOURCE.
I moved the ticket back to the PD team for their comment.
Thanks
David
The tablet is an Apple product..it is not custom. It definitely has a USB controller chip.
Hi Pablo,
I help support the USB PD group. It looks like you're designing a USB device that requires a PD controller to act as the power source to an upstream tablet.
Is my understanding correct?
Thanks,
Matt Schafer
I need the tablet to act as a USB 2.0 downstream facing port (HOST) while still charging (SINK). And we want it to be autonomous. We dont need fancy features. We would like a solution where we can configure with resistors, for example. We dont want to have to configure the ports through I2C.
The tablet must control a single UFP device.
Pablo,
Having the tablet act as a DFP Data-role and Sink Power-role is not a default configuration you can rely on and will require a TPS55288 in your case.
Default (legacy compatability) USB behavior is for the Source to be the DFP and the Sink to be the UFP. This allows backward compatibility with TypeA (DFP/source) to TypeC (UFP/sink) cables. In order to change default startup behavior it requires a device that can do USB-PD which is a large protocol. You can keep it simple by not using all the features and leaving everything default. But the TPS55288 configuration can be made to be autonomous to always try and go into DFP/Sink roles when connected without and outside intervention.
Thanks,
Chris
Is the part number really TPS55288? It seems to be a buck-boost converter. There is mention of PD but not of power roles.

Pablo,
Apologies I definitely meant TPS65988 from Ghouse's comments:
TPS65988
Thanks,
Chris