Part Number: TCAN1462-Q1
hi,
Does the TCAN1462 meet the requirements of ISO 11898-5:2007 physical layer standards?
"ISO 11898-5:2007 High speed medium access unit with low-power mode"
I do not see any mention of it in the datasheet.
Regards,
Keith.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN1462-Q1
hi,
Does the TCAN1462 meet the requirements of ISO 11898-5:2007 physical layer standards?
"ISO 11898-5:2007 High speed medium access unit with low-power mode"
I do not see any mention of it in the datasheet.
Regards,
Keith.
Hi Keith,
The ISO 11898-1:2015 and ISO 11898-2:2016 revisions consolidated all of the -3 through -5 sections into the two section: -1 for protocol and -2 for physical layer. TCAN1462 meets the standard for ISO 11898-2:2016 including the requirements for high speed and low-power modes that was carried over from the 2007 publication.
Let me know if you have any more questions.
Regards,
Eric Schott