Part Number: DS90UB954-Q1EVM
Other Parts Discussed in Thread: ALP
Hello TI support,
I have a setup with DS90UB954-Q1EVM and a self designed PCB assembled with DS90UB953. The two boards are connected via Fakra connector and a coax cable.
The EVM is connected via USB and ALP is running. It's possible to control the GPIO of the 953 by setting the remote register. The test script '953_954_patgen_YUV_1920x1080p-4Lanes-Working.py'
is running well. Also the margin analysis look great.
I load the '953_954_BIST.py' script. After execution time 15.719 sec. there is a text like a report which a I can't interpret. Please see attached file:
My question: Has the script run succsesfully?
Thanks,
Dusan