Part Number: DS90UB960-Q1
Hello all
one of my customers wants to use camera internal ISP output to serializer, DVP 8bit interface, pclk=37.5MHz. And YUV data needs to be transferred. Please help to confirm if the DS90UB933 or DS90UB913 is appropriate.
In addition, the DS90UB960-Q1 has two operating modes, as shown in the following figure, when the raw mode matches 933/913. Can only raw format data be passed? The customer wants to transmit YUV422 data. Do you mind helping to check is it available?