Part Number: TCA9509
Hi Team,
According to customer feedback, in the simulation model of TCA9509, PIN 7 can only be configured as "input", so there is no output signal during simulation. Is there an upgraded IBIS model? Thanks!
Regards,
Hailiang
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9509
Hi Team,
According to customer feedback, in the simulation model of TCA9509, PIN 7 can only be configured as "input", so there is no output signal during simulation. Is there an upgraded IBIS model? Thanks!
Regards,
Hailiang
Hailang,
I'm using the ADS keysight software and when I look at the model (image below), it shows pin 7 as an output.
The SDAB and SCLB channels are technically the same design so if the customer is only able to use SCLB as an output, they can just use two of them and relabel the pin to be SDAB as well.
-Bobby
Hi Bobby,
I'm using the ADS keysight software and when I look at the model (image below), it shows pin 7 as an output.
Could you pls share the IBIS module you have? Thanks!
Regards,
Hailiang
Hailiang,
It's the same one from the product folder: https://www.ti.com/product/TCA9509
In the design & development section of that link.
-Bobby