Part Number: P82B96
One query if you can help me to better understand it.
I believe it is good choice for the design to connect a long cable sensor. The voltage that is available on board is 3.3V. What should be +V Cable? What i should consider while choosing 5 meter cable? I can see different resistance and capacitance values for different lengths. How i can choose these values based on given parameters. VCC= 3.3V +VCable = 3.3V Cable length = 5m What should i consider about the delay in programming because it's seems like this delay might be a problem at some stage? Although, i am simply monitoring temperature through STH30 Sensor, nothing something fancy. Thanks