This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83869HM: Absolute Maximum Ratings for SGMII RX DC Characteristics

Part Number: DP83869HM
Other Parts Discussed in Thread: DP83867CS

Hi,Team

I am looking for DC and UI specification, or Mask for the DP83869HM SGMII.
I found the answer in the thread below.

https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1242254/dp83869hm-does-the-dp83869hm-sgmii-comply-with-the-cisco-standard/4717265#4717265


Please tell us more about the above SGMII DC specs.

[Question 1]
I checked the datasheet, but the SGMII_RX pins (SGMII_SIP, SGMII_SIN)
There was no mention of absolute maximum ratings.
What are the absolute maximum ratings for the DP83869HM SGMII INPUT pins (SGMII_SIP, SGMII_SIN)?

[Question 2]
Please tell me the lower and upper limits of the Vdiff input of the SGMII INPUT of the DP83869HM .
Will it be 800mV, which is the upper limit of the mask specification in the above diagram for SGMII INPUT of the DP83869HM ?
However, if it conforms to CISCO's SGMII specification, the Vi, Input Voltage range will be 675mV-1725mV,
so I think the upper limit of the mask will be (1725mV - 675mV) = +/- 1050mV.

[Question 3]
Are the DP83869HM SGMII RX eye width specifications 0.25UI and 0.55UI in the above diagram?

[Question 4]
We are connecting an AC Coupled Capacitor to the SGMII LINE.
What is the common mode voltage value for the SGMII RX lines inside the DP83867 PHY device?