Part Number: DP83848J
This is our application, we use a cable connection thru RMII bus between two boards.

It is a RMII layout routing, please help confirm the following question:
- The 50MHz external oscillator is synchronized outputted to both DP83848JSQ and DPU, since the lengths of the two don't match, They should be synchronized in terms of clock. Should we make their lengths equal?
OSC - DP83848J : 2" (board 1) + Lsync??
OSC - DPU : 2" (board 1) + 8" (cable) + 10" (board 2) = 20"
If we should do synchronized, we may do fine tune Lsync to 18". correct?
- Extending from the previous question, For Data bus and clock is there any rule for the trace length matching? with in 2"?
- Due to the regulation that the length of signal can’t over 6 inches, but we broke the rule and total length is 10 inches, Is it possible to increase the re-timer or re-driver (model/part number) to solve this problem. Any solution TI suggest?
- Due to we have cable connection, how to tranfer data loss from 6" on board to cable?