Part Number: SN75DP159
Hi team,
if use DP159 as DP retimer, can it support eDP input?
Rayna
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Rayna,
Could you provide more context into the use case of the application such as output and data rate needed?
Thanks,
Zach
Hi Zach,
customer used DP159 as DP retimer followed the guide of application note SLLA358, and when DP input, it works well. But when eDP input, it didn;t work. So I was wondering for eDP input, any configuration need to be modified? Thanks!
Rayna
Rayna,
What eDP data rate are they using? What is the setup for this application?
Please make sure that the device is still in X-mode when the switch to eDP is made.
Thanks,
Zach
Rayna,
Any updates on providing the information requested above so that we can further assist you?
Thanks,
Zach
Hello, Rayna,
I would suggest that you use the DP141 or DP142 and not DP159 for this application.
Thanks,
Zach