Part Number: TUSB216
Hi,
Need your help with the following questions:
- Our total trace length from the USB controller to the end device measures approximately 9.5 inches, while the USB controller's specification allows only 1.18 to 2.95 inches between itself and the transceiver. Is it feasible to have trace lengths between TUSB216RWBR and the end device within the range of 6.5 to 8.3 inches?
- What is the maximum allowable length or loss between TUSB216RWBR and the end device?
- Should serial resistors be placed before TUSB216RWBR, after it, or required in both paths?
Best regards,
Randy