Part Number: SN65LVDS104
Other Parts Discussed in Thread: SN65LVEL11
Hi,
I do not having any experience in playing Video signal like HDMI.
I am asked to design a HDMI splitter, 1:2 i.e one HDMI source input to be splitted in to two HDMI outputs (mirrored).
HDMI outputs are to be connected to two seperate displays (mirrored) having HMDI source input.
1. Can is use SN65LVDS104 to split the LVDS signals of HDMI?
2. Are there any other simple alternatives ICs or designs that TI have to make a splitter design.
Regards,
Harish