Other Parts Discussed in Thread: DS110DF111
I want to use DS110 at 2.125Gbps
Please tell me the register setting.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DS110DF111
I want to use DS110 at 2.125Gbps
Please tell me the register setting.
Hi,
Here are the required channel register writes for this rate.
0x2F = 0x16 (set group 0 to div4 subrate)
0x61 = 0xAD
0x62 = 0x00 (set group 0 rate to 9/4 = 2.25Gbps)
If you are using SigCon architect to configure the device, here is the equivalent high-level device config:

Thank you,
Evan
Dear Evan
Thank you for your answer.
But,I want to operate DS110DF111 with 2.125Gbps instead of 2.25Gbps.
(set group 0 rate to 8.5/4 = 2.125Gbps)
Please tell me the register setting.
Hi,
My mistake, thank you for the correction.
The setting for 2.125Gbps is:
0x2F = 0x16
0x60 = 0x80
0x61 = 0xAA
0x64 = 0xF0
0x67 = 0x00
Regards,
Evan
Dear Evan
Thanks for the corrected answer.
I was able to confirm that DS110DF111 operates at 2.125Gbps with the settings you told me.
Regards,