This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83826I: Collisions in full-duplex.

Guru 11535 points

Part Number: DP83826I

Hi team,

Could you tell me some questions?

1 : When is there a collision in full-duplex (100Base)?
2 : How to use the COL Full-Duplex Enable?
     When there was a collision in full-duplex communication, this register was 0h.
3 : I'd like to set LED2 to blink when collision.
     Is the setting "LEDCFG1(0x460)=0x0140" correct?
     Is it possible to change the blinking of LED2 (on collision) with a setting other than "LEDCFG1(0x460)"?

 BR.
Kengo.