Part Number: DP83826I
Hi team,
Could you tell me some questions?
1 : When is there a collision in full-duplex (100Base)?
2 : How to use the COL Full-Duplex Enable?
When there was a collision in full-duplex communication, this register was 0h.
3 : I'd like to set LED2 to blink when collision.
Is the setting "LEDCFG1(0x460)=0x0140" correct?
Is it possible to change the blinking of LED2 (on collision) with a setting other than "LEDCFG1(0x460)"?
BR.
Kengo.