Part Number: DS90UB941AS-Q1
Other Parts Discussed in Thread: DS90UB926Q-Q1, MIDAS
Hello
- We are trying to use the MIPI DSI signals to drive our display, setup below
Hardware Setup: Quectel SMART-EVB-G2_V1.3 (with SC668S-EM) >>> DS90UB941AS-Q1 (Serializer)>>>via FPD3>>>DS90UB926Q-Q1 (Deserializer)>>>RGB 800x480 Display
What we’ve done so far:
- Use the display driver guide to modify the dtsi files according to the quectel guide (spreadsheet) attached. The following display timing parameters are used:
H = 800
HFP = 44
HSW = 50
HBP = 38
V = 480
VFP = 8
VSW = 3
VBP = 29
Pixel clock = 33 MHz
- For our setup, we’ve determined that changing ili9881 related dsi parameters are needed to have discernable difference.
- Once we’ve changed these two files and rebuilt the android image the touchscreen that it came with stopped working properly as expected; because the timings are different.
- On the serialiser side, we’ve set the following registers:
- MODE SEL [1:0] – this is done via resistors (page 38 of serialiser datasheet)
The current setting is Splitter=0, DSI lanes=4, Clock=1 (FPD link is generated from DSI clock, DSI clock has to be in continuous mode), COAX=0 i.e. twisted pair cabling, DSI=0 i.e. enabled.
- Setup registers set for sync width config as described in page 17 of SNLA356 guide attached
bufW[0]=0x40; //put port select in indirect register 0x40
bufW[1]=0x04; //set port 0
bcm2835_i2c_write(bufW,2);
bufW[0]=0x41; //put address in indirect register 0x41
bufW[1]=0x30; //DSI_HSW_CFG_HI
bcm2835_i2c_write(bufW,2);
bufW[0]=0x42; //put data in indirect register 0x42
bufW[1]=0x00; //DSI_HSW_CFG_HI=0
bcm2835_i2c_write(bufW,2);
bufW[0]=0x41; //put address in indirect register 0x41
bufW[1]=0x31; //DSI_HSW_CFG_LO
bcm2835_i2c_write(bufW,2);
bufW[0]=0x42; //put data in indirect register 0x42
bufW[1]=0x30; //DSI_HSW_CFG_LO=0x30 (48)
bcm2835_i2c_write(bufW,2);
bufW[0]=0x41; //put address in indirect register 0x41
bufW[1]=0x32; //DSI_VSW_CFG_HI
bcm2835_i2c_write(bufW,2);
bufW[0]=0x42; //put data in indirect register 0x42
bufW[1]=0x00; //DSI_VSW_CFG_HI=0
bcm2835_i2c_write(bufW,2);
bufW[0]=0x41; //put address in indirect register 0x41
bufW[1]=0x33; //DSI_VSW_CFG_LO
bcm2835_i2c_write(bufW,2);
bufW[0]=0x42; //put data in indirect register 0x42
bufW[1]=0x03; //DSI_VSW_CFG_LO=3
bcm2835_i2c_write(bufW,2);
bufW[0]=0x40; //put port select in indirect register 0x40
bufW[1]=0x04; //set port 0
bcm2835_i2c_write(bufW,2);
bufW[0]=0x41; //put address in indirect register 0x41
bufW[1]=0x20; //DSI_CONFIG_0
bcm2835_i2c_write(bufW,2);
bufW[0]=0x42; //put data in indirect register 0x42
bufW[1]=0x6F; //DSI_SYNC_PULSES=0
bcm2835_i2c_write(bufW,2);
- Dsi lane config registers to match hardware connections.
- I’ve attached the specs/datasheets accordingly. But unfortunately, the display is not working (we just see a black screen), perhaps you can help us toward the right direction.
Maybe there’s a guide/tutorial that you have that’s applicable to our setup?
Thank you for your time and efforts.
MDT0430E5IHHC-RGB.pdfQuectel_SC668S_Series_Display_Driver_Development_Guide_V1.0.pdf
snla356 user guide.pdf