Hi team,
thanks for your support always!
I have a question here that my customer LIN bus system spec is:
Recommended voltage at pins DSI and DSI_O min to max is 4 to 20V, and Absolute Maximum Voltage Rating is 30Vmax.
Based on this spec, Could we use ESD1LIN24-Q1? how to judge it?
As I know that VRWM is 24V should be fine to use but VBRF will go into 35.5Vmax and the VCLAMP will go into 40V. I'm not pretty sure the energy of ESD test would cause the ESD voltage to breakdown.
BR,
Jimmy