This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9544A: I2C Rise/Fall time measurement timing

Part Number: TCA9544A

Hi 

I have a question on the measurement points for I2C rise/fall time of TCA9544A. 

In the spec, it says the rise/fall time is between 0.3Vcc and 0.7Vcc. 

I have captured the I2C waveform and the base of the waveform is at 517mV.  

Is the rise time measured from 0.99V (=30% of Vcc) to 2.31V (=70% of Vcc) or from 1.352V (=0.517V+0.3[3.3V-0.517V]) to 2.465V (=0.517V+0.7[3.3V-0.517V])?

Thanks.