Part Number: SN65DSI86
Dears,
The maximum MIPI input rate of this conversion IC is 1.5Gbps/lane, and there is only one set of MIPI on my platform. so the conversion chip input is only connected to one set of MIPI, then the maximum is 6Gbps. If my screen resolution is calculated to exceed 6Gbps, can it be driven? Is this input limited? Or only the output eDP side to meet the rate can be (even if it exceeds the conversion IC input rate), the IC does not have an internal buffer, the output can drive a greater rate than the input?
2560* 1600,60 Hz, 24bpp screen, input as long as a group of mipi, can drive?