Part Number: TCAN1044A-Q1
Hi I am studying the possibility of using TCAN1044A into my design.
Just to ensure I understand the standby and wakeup sequence of such chip correctly, let me know if any of my understanding below is incorrect:
- To put the chip into standby is by setting STB pin from low to high logic.
- To wake up the chip I have to
- Put STB pin from “1” back to “0” and
- Generate the wake-up pattern (WUP) pulses as described by section 4.3.1 in order to drive RXD from high to low transition.
Sorry I am a bit confuse with item (b) (ii) above. If there is a dedicated STB pin for standby control, why we can’t wake the chip by simply just pulling STB pin back to 0s instead need the additional WUP sequence?