This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSER953: About FC DATA RATE,CSI BANDWIDTH

Part Number: TSER953

Hi Support Team

I would like to confirm FC DATA RATE and CSI BANDWIDTH.

From Table 7-7, Clocking Modes, when the internal clock is 24.2 MHz in CSI-2 asynchronous mode, the following is correct.
FC DATA RATE :24.2×80=1.936Gbps
CSI BANDWIDTH :24.2×64=1.548Gbps

7.4.1.3 Non-Synchronous Internal Mode states the following at 24.2MHz.
Are these values correct?
FC DATA RATE :3.872Gbps
CSI BANDWIDTH :3.1Gpbs

Best regards.