Part Number: TSER953
Hi Support Team
I would like to confirm FC DATA RATE and CSI BANDWIDTH.
From Table 7-7, Clocking Modes, when the internal clock is 24.2 MHz in CSI-2 asynchronous mode, the following is correct.
FC DATA RATE :24.2×80=1.936Gbps
CSI BANDWIDTH :24.2×64=1.548Gbps
7.4.1.3 Non-Synchronous Internal Mode states the following at 24.2MHz.
Are these values correct?
FC DATA RATE :3.872Gbps
CSI BANDWIDTH :3.1Gpbs
Best regards.