This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB638-Q1: Design documents support for DS90UB638-Q1

Part Number: DS90UB638-Q1


Hi Team,

Please help to support the layout guide, reference design schematics, and initial code,... to help the customer.

I cannot find related files on the website.

customer application is 9” Side Mirror System

9” High Resolution Panel-1920 (H) x 720 RGB (V)

Power Input: 9~36V

Camera Input Source

LVDS-TI658 (Camera-953 Input included ISP, YUV output )

Thanks.

  • Hello Peter, 

    Firstly, please note the DS90UB638 is not compatible with the DS90UB953. To use the DS90UB638 in your system, please select the DS90UB635 or DS90UB633A serializers. 

    Reference design schematics can be found on TI.com under the Design & Development tab. The reference designs can be searched with additional filters to reference ADAS FPD-Link devices as linked here: TI Reference Designs FPD-Link ADAS

    Depending on the application, with the hardware set up correctly, the devices will be able to lock without any software configuration required. Information on necessary hardware is shared in the datasheet of the device. Important considerations regarding the application include the device mode, and CSI-2 forwarding as examples. The datasheets provide example scripts for specific functions such as configuring Pattern Generator, CSI-2 forwarding, and GPIOs. 

    Please let me know if you have any additional questions. 

    Best,

    Zoe