Other Parts Discussed in Thread: TLK10034, MSP430F5529
Hello,
My customer is looking to use the USB-2-MDIO GUI and MSP430F5529 LaunchPad to communicate with TLK10034. They're able to read registers from the TLK10034, however, they're running into an issue when trying to change the Device Address field per the TLK10034 datasheet. There does not appear to be an option to do this in the USB-2-MDIO GUI. Are we missing it or is this functionality not supported? What would you recommend here?
Note that the value of Device Address, DA[4:0] for the TLK10034, depends on if you're in Clause 45 or Clause 22 mode as well as the registers you're trying to access. Therefore, they'd like to be able to adjust DA[4:0] to be able to access certain registers. How can they do this with the USB-2-MDIO?
Thanks in advance for your support.
Best Regards,
Brian