Part Number: SN75LVPE4410
We want to add a redriver for the PCIe signals going between two card modules via a backplane. In the top half of the attached PDF block diagram, we were able to connect the PCIe channels between the cards without redrivers and without any additional capacitance other than on what is already mounted on the left-side card without any major issues (so far) on a much smaller prototype.
When incorporating the SN75LVPE4410s to redrive, what is the recommendation for where to place any AC coupling capacitors? Currently, I have them only on the "right" side of the redrivers (i.e., on the TX/RX going to the right-side card, marked in red in the bottom half of the PDF), but I'm not sure if that's correct since the SN75LVPE4410 specifies that they should be placed close to the RX pins. Should only the AC caps on the TX pins be specified >1in away from the pin, while the RX pins should be as close as possible?
Additionally, the switch specifies 100nF capacitors to be placed on every TX and RX line, whereas the SN75LVPE4410 recommends 220nF. Is having a capacitance mismatch problematic?
Thanks for your help,
Gillian