Hello.
I am using DP83869HM in 1000M media converter mode. Actually there is no problem with communication and data transfer, but
I'm wondering if LED #2 is not blinking.
The operation of the LEDs is as follows when the SD signal is detected, the link is connected, and data is sent and received.
LED_0 : Solid
LED_1 : Solid
LED_2 : Solid
I know that most Ethernet ICs indicate TX/RX ACTIVITY by flashing.
Is the behavior of LED_2 blinking or solid?
Additionally
Could you please check if I am doing something wrong with the LED band settings?
Sincerely.