Hello,
The following figure is a partial block diagram of the product:

During normal operation of the product, the MCU resets the SOC.Then the SOC will turn off the POC power supply of the camera and then power on (TI935 and image sensor will be powered off and powered on). However, during this process, the power supply of TI936 has been normal and there is no software reset. At this time, TI935 will report a fault CSI ERROR(as following figure), and TI936 have no MIPI signal output.
So, SOC can not detect the MIPI signal and reset the camera again. TI935 will not report a fault CSI ERROR, but TI936 still have no MIPI signal output. Now, if the SOC sends a reset command to TI936 , the MIPI signal output is normal.
May I ask what are the possible causes of the above problem?