Part Number: DS320PR810
Hello,
What is the input current requirement for the PCIe redriver?
Regards,
Nachiketh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS320PR810
Hello,
What is the input current requirement for the PCIe redriver?
Regards,
Nachiketh
Hello Nasser,
So according to this maximum current required will be around 600mA?
Regards,
Nachiketh
Hello Nasser,
1. If RX_DET is disabled, will the redriver work for both the TX and RX signal flow attached, Root Complex is PCIe compliant.

Regards,
Nachiketh
Hi Nachiketh,
Yes maximum current of 600mA is good.
You can disable RX_DET. Please note there could be interoperability issue between root complex and the end point - this depends on these two entities. In PCIe specification, root complex and the end point expect RX_DET to be enabled. Additionally there is PERST# signal for synchronization purpose. I am not sure how you are planning to bring this signal across fiber connection.
Regards, Nasser