Part Number: TCAN1043-Q1
Other Parts Discussed in Thread: TCAN1043
Hi,
About rise time and fall time of TX,RX,CANH,CANL, one customer ask to follow the spec related to data rate. That is <10% of the period(1/data rate). When data rate come to 5Mbps, the CANH and CANL can not meet the requirement which is 20ns no matter how we adjust the circuit.
Is this request reasonable?
And is the device possible to drive CAN bus that fast?