Part Number: DS90UB941AS-Q1
HI TI experts,
Are there any problems if the FPDlink passes the margin analysis program (MAP) test but fails the input clock jitter test when using DSI as REFCLK ?
How should I assess the functionality of the FPD link based on the MAP test results if they all pass?
Here are the conditions in my test :
Configuration :
1. Single FPD link
2. Pixel clock : 36MHz
3. DSI clock : 108MHz, 4 lanes
4. FPD link length : 3m
From the above configuration, the maximum allowable total jitter is approximately 238ps. However, the measured total jitter can reach up to 250ps.