Part Number: TUSB2046B
Hi TI!
I am designing a system that can connect N devices via USB. Each device has an MCU that has a USB interface (MSP432) and is powered by an external power supply independent of USB.
I show the connection diagram of 4 devices in an attached image.
1-) The diagram presents a possible topology for the TUSB2046B? Can several TUSB2046B be connected consecutively (as the diagram)?
I also attach my wiring diagram for the TUSB2046B.
2-) Is the schematic correct?
Note: since the power supply of each device is external I do not use current verification so:
OVRCURs on high pull up
PWRON unconnected
I use 6MHz crystal
BUSPWR to GND
Thanks very much!