Part Number: TCA9509
Other Parts Discussed in Thread: TCA9517
Hi There,
I plan to use the TCA9509.
Please let me know if there are any mistakes in usage.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi User1881876,
The TCA9509 is being used incorrectly! A-sides are tied together which cannot happen for this device due to internal current source on the A-side. In an application where the customer needs the contention side to be on the B-side, consider switching to the TCA9517 which implements a static voltage on the B-side.
One of the main reasons A-sides cannot be tied together is because of the internal current source, which is used to tell the buffer when side is driving a low-logic signal in order to prevent lockup on the I2C bus.
Another reason is that the output low voltage produced by the buffer on the A-side when a valid low logic level exists on the b-side input is not low enough to reach the input low contention voltage on the A-side. VOLA (typ) = 0.18V while VILC(typ) = 150 mV.
Regards,
Tyler