Part Number: THVD8000
Hi,
I'd like to control the digital side of the THVD8000 with just two wires, so connect R and D pins together, and select the direction using MODE. This requires the R output entering high-impedance mode when MODE=1. Of course, my microcontroller also changes direction accordingly.
The data sheet contains a row defining I(OZ), "Receiver high impedance output current", but here the "test conditions" are defined as "... Mode = 0". This confuses me. The receiver output can't be in high impedance mode with MODE=0.
So does the R output enter high impedance mode in transmit mode, set by MODE=1 ?